This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AIC3262 miniDSP programming and changing EQ

Hi Team,

 

Can you confirm the following regarding the AIC3262: 

  • The miniDSP can only be programmed via the PurePath GUI
  • How are the algorithms (like the dual mic noise reduction) implemented? Only via the GUI?
  • Is the AIC3262 EVM suited to evaluate the dual mic algorithm?
  • Can the EQ settings can be changed on the fly via I2C register settings?

Thanks.

Regards,

Adrian

  •  Adrian,

    • The miniDSP can only be programmed via the PurePath GUI
      • Yes.
    • How are the algorithms (like the dual mic noise reduction) implemented? Only via the GUI?
      • D-mic NC is not supported any longer.
    • Is the AIC3262 EVM suited to evaluate the dual mic algorithm?
      • You can connect two microphones, but the algorithm is not available.
    • Can the EQ settings can be changed on the fly via I2C register settings?

    Regards,

    J-