Hi Sir,
I am Aravind working as FAE. I suggested the part TLV320AICV3254 to one of my customer. They gone through datasheet and mentioned me that using this device by means of programming either the line o/p or speaker o/p can be taken at a time. But they actually needs all the 4 outputs to be simaltaneously available at a time. What i have to do now. Kindly help me on this issue. If the device not supports all the 4 o/p's at a time, then is there any device from TI can support this option, kindly need help.