Other Parts Discussed in Thread: TLV320AIC3204
Hello,
I want to use TLV320AIC3204 for beep generator only for the moment.
I have a hardware question. I use a µC connect only with SPI to the TLV320. I don't use I2S pin.
My output is on LOL pin.
SPI_select pin is High.
LDOin, IOvdd, and LDO_select pin are to 3.3V.
I try several initialisation but nothing works.
I have 1.7V on Avdd and Dvdd pin, but I have 0V on REF pin.
Can you see the problem ?