Hi,
we have a strange phenomenon with the AGC of the AIC24 Codec: The target level seems to be dependent on the sampling rate. Our measurements with 1kHz input signal: 48 kHz sampling rate result in ~71% level, 44.1 kHz in ~68% and 22kHz in ~33%.
We cannot find appropriate infos or formulas in the data sheet, so can anybody please explain us the dependency of the AGC target level on the sampling rate and how to calculate the target level correctly?
Thanks and best regards
Roland