hi everyone,
how can i transmitt serial data from the master over the datasidechannel and how is it possible to set or get the digital ios from the slaves?
thanks for answers, best regards
hubijo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi everyone,
how can i transmitt serial data from the master over the datasidechannel and how is it possible to set or get the digital ios from the slaves?
thanks for answers, best regards
hubijo
Hi Jonathan,
Have you read about the data side channel in the CC85xx Family USer's guide? http://www.ti.com/lit/ug/swru250l/swru250l.pdf
Chapter 3.4.4 describes the data side channel in detail. Pleas let me know if you have any further questions.
Itæs possible to map slave GPIOs to master GPIOs (if that is what you want). To do this you go to the master and slave User Interface panel and check so many functions as GPIOs you want to monitor. It is important that you select the same functions on both slave and master. Then you go to the IO Mapping panel and map these functions to the corresponding GPIOs.
A short example:
If you want the master's GIO2 and GIO4 to reflect the slave's GIO1 and GIO3 you do this:
Hi kristoffer
thank you for the answer. It means i can map the gios from the master to the slave ands et it as an output or input?
Which pins should i connect to transmit i2c serial data or spi?
Best regard hubijo
Hi Jonathan,
The wireless GPIO transmission is only possible from slave to master. All your questions are answered in the User's guide, but I2C is the SCL (32) and SDA (33) pins. SPI is CSn, SCLK, MOSI and MISO at pins (3-6).
-Kristoffer