This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Driving Multiple TPA6130A2

I am connecting the same single ended signal to the input (pin 1) of several of these chips through a capacitor (pin 2 is connected to ground through a capacitor on each chip).

Can I connect this signal through 1 capacitor and then to all of the pin 1s of each of the chips where I am basically tying all of the pin 1s together? Or.. do I need a separate
cap on pin 1 of each chip connecting it to the input signal?

I can save quite a few caps if I can tie the pin 1s together but I'm not sure if they would end up fighting each other since they each apply a bias to the input pin.