Hello,
We are designing an audio streaming system with the CC8530 and the CC2590.
we deisgned the PCBs to be 4 layers, almost exactly like the modules that come with the cc8530 evaluation kit.
The problem is that we can't get the same range as with the kit, and our antenna is very sensitive. we can't go beyond 10 meters, and at that range, anyone getting close it causes the connection to be lost. Strangely, in the same conditions, the evaluation module is much more robust.
In this post, i would like to expose the differences between our PCB design, and the one of the evaluation kit. Could any experienced user or TI expert tell me if those differences could be causing the poor performance of our RF link?
1- The isolation of the GND plane around the trace going to the pcb antenna in the not the same. it's much bigger on the evaluation kit (black) than on our pcb (blue)
2- On our PCB, the antenna itself is not on the same layer as CC2590 and all other components. As you can see in the image below, under the yellow circle, the antenna signal goes from the bottom to the top layer.
(on the image below, the GND planes are hidden on purpose to make it easier to see the tracks)
3- Finally, we have less GND vias around the CC2590 than on the evaluation board.
We are going to design new PCBs, do you think only those 3 points need to be corrected? can you think of anything else that can maximize our chance of having a robust radio link?
Thank you very much,