Other Parts Discussed in Thread: DAC1282
Hello,
I was over in: http://e2e.ti.com/support/microcontrollers/c2000/f/171/p/303479/1059565.aspx#1059565 and it was suggested I ask the question in a couple of the other forums.
You can refer to the above link for background - question is achieving 24-bit resolution and accuracy for a control loop - in this case for an EFC for an OCXO.
Is there a low-speed Audio DAC that would work? In the past the Burr-Brown PCM61P was used in this design - that was only 18bits but that design had a manual pot also for that reason I suppose.
I have looked at the available DACs - some are nice in that they have a glueless interface to the 28069 (McBSP) - but is it a good way to control a noise sensitive circuit like an EFC for an OCXO?
Alternatives are PWM (don't think the real bit resolution can be 24 with the 28069) and putting two 16-bit DACs together with the proper weighting for the resistors through a summing op-amp.
I should add that the output voltage should be a held DC mode like the DAC1282 has.
Suggestion appreciated.
Thanks,
johnw