I am trying to achieve the maximum possible range with PurePath. I think that the best parameters for this would be 2 Mbps RF data rate, Mono, 32 kpbs audio bit rate, with PCMLF encoding. Is this correct? Is there a way to disable (or change the coefficients of) the antialias decimation filter for the PCMLF encoder? If not, what is the relative performance of the SLAC encoder versus the PCMLF encoder?
Thanks!