Other Parts Discussed in Thread: TPA2015D1
Hi,
My customer is having problem now on efficiency measurement on TPA2015D1EVM.
As long as they test this EVM, they can achieve around around 400mW Pout, but datasheet specify max output is around 2W.
Based on the guide line of audio performance measurement app. note, I'm still supporting customer.
http://www.ti.com/lit/an/sloa068/sloa068.pdf
Here is their conditions.
---
Load: 8ohm + 33uH
input: 1KHz single ended
VBAT: 3.6V
AGC: floating (no infection point)
GAIN: high (20dB)
---
So far I could not see any of suspicious on their evaluation set-up, except a resistor R4 is 0ohm.
(In the schematics of EVM, it's mentioned that R4 is 1kohm.)
Since customer use the function generator as input source with single end at JP IN jumper, they don's use RCA connector,
so left side of C1 is already short circuit to GND via JP SE jumper.
I still don't know why this happen, but do you think this is the reason why customer can't have enough output?
Sorry for less information, but it's appreciated if you give some comments on this matter.
Thanks,
Ken
tanaka-k@clv.macnica.co.jp