This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can any one help with the standard test for 70V amp!!



We just bought a 70V (50w)amp for the testing, should we run the full load for 6 hours or 1/3 or 1/2 load for 6 hours?

Is it right testing with following condition:

By testing the 1KHz(316mV) with 98 ohm loaded.