I have recently come across a Microchip announcement of their Bluetooth audio solution capable of 16/24 bit up to 192 kHz audio bandwidth. Up till now I have thought BT A2DP has a maximum bandwidth of 768kbps so Purepath is about the only "open" technology for CD-quality streaming. But there might have been some new BT developments and it can handle HQ audio transmission. Documentation available at Microchip is not very detailed and somehow I feel it might not "work as advertised". TI also has BT chips so I would appreciate some explanation what differences there are between the two technologies and what are Purepath's advantages over a HQ audio BT technology.
That would help me stay firm with Purepath my developments.
Regards, Pawel