In an application with the TPA3118D2 ic. I am getting my ICs to go into a fault where they cannot get out. For instance, I can connect my audio inputs and power supply to the IC and it functions great even at very high loads. After a few (10 or less) connects and disconnects the IC goes into fault mode, tries to self clear, but never does. So I get the 1 hz enable disable problem. I have looked at different threads and disconnected my output capacitors, tired different ones too and measured for shorts to my outputs. Everything came up good. Is the ic dead or can this problem be fixed? I have mute tied to GND. SDZ and Faultz are tired to a 100k pullup. I almost directly copied the typical application circuit from the datasheet.