This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320DAC3203 support --- NO MICROPHONE INPUT with ADMP421b

Other Parts Discussed in Thread: TLV320DAC3203

Hi TI sir,

We met problem with ADMP421 and TLV320DAC3203. No any audio data checked by oscilloscope.

MICBIAS is provided by AVDD 1.8V and configure REG 0x33 with HEX 0x50 -- means MICBIAS is 1.7V. The other DAC3203 configuration follows user guide. But we can't get any audio data from MIC.

Please give us some advice.

DAC CONFIG:

#----------- Initialize to page 0
w 30 00 00
#----------- Initialize the device through software reset
w 30 01 01
#----------- Set PLL_CLKIN as MCLK and CODEC_CLKIN as PLL_CLK,
w 30 04 03
#----------- Power up pll, set pll divider P=1 and pll divider R=1,
w 30 05 91
#----------- Set pll divider J=8
w 30 06 08
#----------- Set pll divider D=0000
w 30 07 00
w 30 08 00
#----------- Power up and set NADC divider = 2,
w 30 12 82
#----------- Power up and set MDAC divider = 16
w 30 13 90
#----------- Set AOSR = 64
w 30 14 40
#----------- Select page 1
w 30 00 01
#----------- Disable internal crude AVdd in presence of external AVdd supply
#----------- or before powering up internal AVdd LDO
w 30 01 08
#----------- Enable master analog power control
w 30 02 00
#----------- Set the REF charging time to 40ms
w 30 7b 01
#----------- Select page 0
w 30 00 00
#----------- Select PRB_R2
w 30 3d 02
#----------- Configure MISO as clock output for digital microphone
w 30 37 0e
#----------- Power up left ADC and right ADC. Enable digital microphone mode for left ADC
#----------- and right ADC. Treat data on SCLK as digital microphone data
w 30 51 dc
#----------- Unmute left ADC and right ADC
w 30 52 00