This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Purepath Wireless input switching

Hello I was wanting to know can the CC85XXDK-HS Wireless system allow audio input switching from either the line input or USB on the fly to send to headset?  Also inversely can output be monitored on usb while using the line input -> wireless?  I'm allready using a 2902 dac just wondering if the wireless package can replace it.

Thank You

Jay Steele

  • Hi,

    It is not possible to switch between line input and USB on the fly. The device is either configured as an USB audio device or a “standard” audio device, to switch between these configurations the device must be re-programmed with a new configuration.

    No USB communication is available when the device is configured as a standard audio device.  

    Best regards,

    Johan