Other Parts Discussed in Thread: PCM9211
Hi,
I have an I2S 16-bit 48 kHz Stereo audio source wired to a CC85xx TX and transmitting just the Left channel data to another CC85xx RX across the room. Assume I set that latency to 768 samples. The Right channel I2S data doesn't go over the RF link, and just remains on the TX side where it must eventually go through a DAC.
My problem is... I need to delay the Right I2S stream too by 768 samples before the DAC so it remains in sync with the Left. Can the CC85xx do this "I2S delay" function for me? I see it has three I2S data i/o lines...
No doubt this delay function will eat up the memory. What's the max I2S delay (with matching latency) we can use in such a setup?
Thank you in advance.
Andrew