Other Parts Discussed in Thread: CC8531, CC2591, CC2590
Hello
I have a issue with control signals from CC8531. I make my own design of the board. Here is schematic. CC2591 and CC8531 is connect following the reference design.
In PPW Configurator I set in radio range extender- CC2591 HMG.
Than i measure logical states on EN and PAEN signals:
On master device in: standby mode: EN=0 , PAEN=0
pairing mode: EN=0 , PAEN=0
On slave device in: standby mode: EN=1 , PAEN=0
pairing mode: EN=1 , PAEN=0
Of course the devices can not pair together.
When I set in range extender option- none, than the devices are paired together, but the connection is very weak and crashing down .
Why are the control signals incorrect ?
Thanks for answers.