Dear Friends,
I used two ADCs of MSP430F2619 to monitor the outputs of TPA3132D2, the TPA3132D2 worked fine. The ADCs of MSP430 were saturation at maximum voltage 2.5V when I connected it to a 12V or 19V power source, however, if I connected it to a 5V power source, everything worked as what I expected. Does anyone have the same experience on this issue?