This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3106 example muddles channels and makes 6 dB attenuation

Other Parts Discussed in Thread: OMAP-L137, TMS320C6747, TLV320AIC3106

Dear E2E Community!

I'm trying to configure TLV320AIC3106 at OMAP-L137 EVM (I use it for debugging a software for TMS320C6747 DSP). I shall use an TI (Spectrum Digital) example "aic3106" as the template for my configuration program. But I can't understand why? :

1) at the stage "Audio Loopback from Linein [P10] --> to HP/Lineout [P12/P13]" (execution of the function aic3106_loop_linein( ) ) the device muddles left and right channels;

2) during working of the same loopback-program, device attenuates output signal relative to input (6 dB). PGA Gain is set to 0dB, Gain LINE1L to  Left ADC and LINE1R to Right ADC are set to 0 dB also.

I shall be very appreciate for any advice! Vitalii PS: Example (test) project "aic3106" is part of the archive

http://support.spectrumdigital.com/boards/evmomapl137/revg/files/revg_EVMOMAPL137_BSL.zip

Unfortunately I can't understand, how to attach the archive with project to the message.