This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5548 _PLL gound Layout

Other Parts Discussed in Thread: TAS5548

Hello

Customer intends to use TAS5548.

Customer pointed out that  there are PCB layout  in the TAS5548 EVM slou351b.pdf.

According to that document, PLL ground  #5 pin is connceted to DVSS with trace ( 0 ohm).

Anyway , in the previous   PWM processor TAS5508  data sheet sles257.pdf , page 102 there are  description

that AVSS #5 pin(PLL ground )  should be connected  to GND with 3.3 ohm.

Do you think  Customer should follow as TAS5548 data sheet? Or

PLL gound #5pin has better to connect   to DVSS with 3.3Ohm as SNR point ?

Please advise