I am finalizing quite ambitious commercial audio project and one of its important features is HD audio quality over radio link using CC85xx. It is, however, only possible using 2.1 PCM configuration. For over two years I have lived in belief it is possible using CC85xx as I checked this configuration in PPC. Now I am ready to testing and it has turned out it is probably not going to work since it is possible on the Master side.as I checked but it has just turned out to my great dissapointment that 2.1 config is not available on the Slave ... I understand my config, i.e. 2.1 Master to 2.1 Slave is not one of the "use cases" defined by CC's designers. But the bandwidth is there, the firmware modification is slight if any - could you please add 2.1 configuration option to PPC on teh Slave side ? There is already a 2/1 Slave config available that allows to configure 3xPCM16 so the only change is 2.1 output channel instead of 2 out/1 in.
I would also like to remind of my earlier post and question also concerning the 2.1 mode - the user guide discourages from using it - what practical disadvantages or negative impacts I should count with when using it ?
As this issue seems quite straightforward to address while it is quite important for my business success in using CC85xx chips I would appreciate an answer possibly soon here or even better directly by e-mail off-the-forum.
Thanks, Pawel