This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About TAS5717's DSP

Other Parts Discussed in Thread: TAS5717

Hi members.

This is BEN.
My customers is using TAS5717  for monitor.
It is a question to success with further TAS5717 for the next model.

《Q》
 TAS5717 is include  a  DSP.
   How  quantization accuracy  are  either  constituted  by the DSP ?

◆For example
    I suppose the datasheet p31【26-bit 3.23 Number Format】.
    ・sign 1bit  ,   integral 2bit ,  point-unit  23bit
 Is there any room in the head ?  2bit(12dB)?

 

Best regards
BEN.