In the electrical characteristics the measured bandwidth for the parameters is from 20Hz to 20kHz, and at the bottom it says the bandwidth is limited by using the Audio precision 22Hz high-pass filter.
I am curious if this will work in an application for frequencies from .1Hz to 20kHz with the high pass filter disabled with the HPFD pin?
More on that, what will the device behave like in the frequency range .1 - 20Hz if that will work?
If this part won't perform well in that lower range is there another ADC that is good for the above bandwidth?
Thank you!
Zach