Other Parts Discussed in Thread: CC2541, CC2543
I am interested in using a PurePath chip, but was wondering how many I could use without an issue? The setup will be one master to one slave running mono audio. Can I have multiple sets of masters and slaves running in the same area without issues? Is there a maximum number I can have? For example, I have 1 master and 1 slave for each channel of 7.1 surround and the respective speaker, so there would be 8 total sets of PurePath connections in one area.