Other Parts Discussed in Thread: PCM5142
Hi,
Just new to PurePath and the miniDSP engine on the TI chips, and am having some issues.
I created a very simple DSP filter, that just switches the left and right channels from the input to the output. I then build this code and use the output cfg file to program the registers in my TI PCM5142 DAC correctly (using my host micro).
Everything works, when the DSP filter is engaged, the left and the right are switched. However, it only works up to 192 kHz (and the DAC supports up to 384 kHz). Whenever I give the DAC 352.8 or 392 kHz I2S data, I don't get any audio output. Attached is the filter in PurePath.
I've also tried the "Int8xOutROMsl" component, and same thing. It seems that I need a "Int16xOutROM" component, but there isn't one, or is this barking up the wrong tree?