HI
Does the TAS5727EVM & TAS5721EVM comes with the MC57xxPSIA and USB-Inpput board 3 respectively?
It is not mentioned at allin the user guide
Ivan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
Does the TAS5727EVM & TAS5721EVM comes with the MC57xxPSIA and USB-Inpput board 3 respectively?
It is not mentioned at allin the user guide
Ivan
Hi, Ivan,
Yes, those two EVMs come with the target and controller.
-d2
Hi Don
Thanks
To clarify, controller board is the board which allow the user to connect to PC and the analog in and digital out?
For TAS5721EVM it is known as Input USB board 3
For TAS5727EVM it is known as MC57xxPSIA
Are they the same boards and can they be used vice versa
Ivan