This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Single IC Split Rail



Hey

I have a circuit with several OP-AMP's and I wish to power them on a single voltage supply. My project time is limited and I do not wish to waste time reinventing the wheel and build a circuit to get a reliable dual supply. So here is my question: Is there any single IC that I can get to take a voltage say +12V and split it up into +6, VGND and -6 (anything similar will also make me jolly).

I require a current of round about 500mA maybe more. I have to amplify signals that are up to 200kHz.

If you can, please, PLEASE help

Thank you