Hi,
Im planning to feed my PCM1794A with I2S data. As far as I see the PCM1794 uses the clock source from the I2S Signal. Now when I switch the Sources the Clock also changes. Is that a problem or do I have to use one clock Source for all the devices (DIR9001 and PCM2707)?
Is it possible to use a "master clock", for example the PLL1708, to generate a master clock Signal for the whole I2S Net?
How do I have to supply this clock? Using the SCK0 Output from the Clock Source and supply it to all BCK inputs?
I have two masters, the PCM2707 and the DIR9001 and one Slave (PCM1794A). My plan was to switch between these two with the 74HC157D.
Or is this the totally wrong way and there are other/better solution for my problem
regards
Patrick