This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello:
I'm isung a PCM2906C to interface with a SPDIF interface codec that works at 48 kHz only. The default volume control in Win7 does'nt do anything in the SPDIF output of the PCM2906C. The default mute control neither.
The application (Windows Media Player) volume control and mute control works fine, but it's not the default volume control. Is there any way tho do working defualt Windows 7 volume control?
Thanks in advance.
Hi, Santiago,
My understanding is SPDIF is a line-level signal, and thus, volume control won't affect it.
-d2