This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA2006D1 driving a 4 ohm speaker at 5 V

Other Parts Discussed in Thread: TPA2006D1

I have a circuit designed around the TPA2006D1 amplifier driving a 4 ohm speaker.  The amplifier is sources by a 5V supply.  It has been run in development intermittently for several months without issue.  I am not using the full power  output of the amplifier - in fact, I am probably only at about 200 mW of power output.

However, I just noticed today that I have a problem.  In the datasheet, there is mention in the max settings section that the minimum load resistance above a 4.2V supply is 6.4 ohms.  I assume this is due to the fact that there is not enough resistance to the output FETs and it could weaken them with a lower load resistance so even though I am not using the full power of the device, I would still have problems.

I can't find an 8 ohm speaker that meets our needs.  Is there anything that can be done to allow the use of the 4 ohm speaker?  I have thought of putting a diode in the power supply path to drop .7V to get it closer to the 4.2V.  I thought of adding an inductor in series with the speaker to bump it's effective impedance.  Would either of these work?  Is there a better way?  (Or any way?)

Thanks,

Brent