This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

msp-expf5436A sample music with ADC

Other Parts Discussed in Thread: MSP430F5436A

Hello,

I want to sample audio with internal ADC of the msp430f5436A.

As i understand, the music goes out of the PC (through the 3.5mm PL - Auxilary Connection) is 1V max and -1V min.

Also, as i understood , the ADC of the msp430f5436A can sample waves between 0V and 3V.

Is there a way (or a module) that can bridge the voltage, such that it's input will be [-1V,1V] and the output would be [0V,3V]?

Hope that is the right forums,

Thanks.