Can purepath wireless configuration like real two-way wireless communication? one master talk and listen with slave, see attached.
CH
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can purepath wireless configuration like real two-way wireless communication? one master talk and listen with slave, see attached.
CH
Hi,
PurePath supports bidirectional audio. If you are using a network with one master and one slave it is possible to stream 2 audio channels from master to slave + 2 audio channels from slave to master.
Regards,
Johan
Can I use CC85XX for multichannel listening systems?
Number of channels 10 can be.
For example 10 transmitters, and 1000 receivers. And user can select channel from 10. Receiver and Transmitter using 85xx IC
Hi Alex,
PurePath only supports star networks consisting of 1 master and up to 4 slaves. It is not possible to have a larger networks than that. The four slaves in each network can select which channels transmitted from the master (max 4 channels can be transmitted) to receive.
Johan
Hi Johan.
1) In my System Master needs to send Audio to 6 slaves. Here all slaves may configure to same channel all different channel but at a time Master will be communicating to single slave.
2) Also Master can change its Channel frequency to communication with slaves if they are configure at different channel. So I need to reconfigure Master using SPI.
3) Also Slave can change its frequency . So I need to change its frequency too.
Can I use CC8530 for my application. Because I am confuse with Channel number. Also need to know about range. I need 100 meter range for my product.
Regards,
Meet