This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AIC3204 Mono Differential Outputs without ADC & DAC digital path.



Hi,


I have a simple application that requires doing an analogue audio route of 2 differential line inputs (IN2 & IN3) to 2 differential line outputs (to HP & LO) on the AIC3204.

I know the RDAC can make an inverted version of the LDAC, but if possible I would line to not use the digital path and reply simply on the analogue path such as the MicPGAs, the MAR/MAL and the respective output amplifiers such as the LO & HP amps. The LOR output can be fed back into the LOL input, and the HPL can be routed back into the HPR input, but doing this will it also invert the signal to allow for differential signalling on the outputs ? Otherwise woud I need to use the digital path instead and then use the inverted RDAC signal copy of the LDAC etc ... ??


Thanks in advance for any clarification.

mke