We are using a TPA3110D2 in an application where the supply voltage can vary over a wide range, as high as 40 V, which exceeds the absolute max for the amplifier (30 V).
To that end we placed a clipping circuit (below) before the amplifier to prevent it from seeing more than about 23 V.
I am finding out rather late in the design cycle that this clipper is subject to rather extreme oscillations (40 dBuV) in the 60 kHz range. These are most noticeable at the point where the zener diode first turns on, but it continues to oscillate even at higher voltages when I would have thought the transistor was full on. We tried adding capacitance between gate and source and across the diode but they make no difference whatsoever.
The oscillation has no effect on circuit operation, but causes us to fail an emissions test--a variant of CISPR 25.
We have tested the circuit shown, completely removed from the application and found the oscillation changes shape but remains a problem over a wide range of load currents.
Has anyone else had to limit the supply voltage for this part and if so, what approach did you take?