This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

lm4780

Do each amplifier of the LM4780 has an independent following key specifications:

1• Output Power/Channel with 0.5% THD+N, 1kHz into 8Ω: 60 W (Typ)

2• THD+N at 2 x 30W into 8Ω (20Hz - 20kHz):

0.03% (Typ)

3• THD+N at 2 x 30W into 6Ω (20Hz - 20kHz):

0.05% (Typ)

4• THD+N at 2 x 30W into 4Ω (20Hz - 20kHz):

0.07% (Typ)

5• Mute Attenuation: 110 dB (Typ)

6• PSRR: 85 dB (Min)

7• Slew Rate: 19V/μs (Typ)