This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

shutdown control when no audio signal

Dear

I have tested my project with class D amplifier TPA2005 and TPA2012.

The project is very simple, as belows: 

audio signal input (mainly smartphone music player, mp3 player) -> amplify -> speaker.

My prototypes are working well, but I want to add "shutdown function when no audio input signal."

I did some tries with comparator, transistor etc....but not satisfactory.

Could you recommend any simple methods? 

I want to make this as simple as possible to save PCB size and manufacturing cost.

(MCU is also not available.)

Thanks very much in advance.