Hello All,
I built a simple buffer circuit using a LME49710. I chose the device for its high input impedance and also because it did not require offset nulling. It sounds good but I encounter a strange behavior when the circuit is disconnected from and then reconnected to the power source (single supply, regulated 9VDC). The circuit does not turn fully on (very low output, lower than unity). It would require for the circuit ground to be disconnected from the power supply ground to "reset" the circuit and enable it to fully power up. Could this be because the op amp is designed for dual-supply and I am using it with a single supply? Is there something I could do to make it work with a single supply? I could post a schematic if that would help.
Thanks