Dear TI community,
we are currently on search for a developper board that fits our needs.
As it seems until now, this special board is very difficult to find.
Especially the size makes it very hard, because the Dimensions should be max. 2,36 x 2,36 inches.
What we need:
- OS: Linux or Android
- Audio Line In
- Slot to increase the memory of the device (SD Card or USB)
- USB to charge the Battery (battery powered device)
- Battery connector
- Bluetooth
- Power Button
If theres not only one board that fulfills these needs, a solution with two boards (each max. 2,36 x 2,36) connected together would also be possible. Please keep in mind, that we are at the starting point of developping products. Thanks so much!
All the best!