Other Parts Discussed in Thread: TLV320AIC32
Hi, All
I am using TLV320AIC32 codec with DKWT32i-A Bluegiga kit. I want to generate some filters of EQ mode, like JAZZ, ROCK, BASS. and etc., but I can't.
The communication between BTI module and TLV320 are through I2C and I2S. I send data like this "30 18 0200918000008A1037000100008000000FF07C7C787C7C78 30 04 25C01400 30 0a 28C00000000000008000 30 03 330F00 30 05 3F00800F00 30 04 6500A200" to the codec.
“30” is the 7-bit I2C address of the external codec device shifted left by one. Bit 0 should be zero.
“18” is the number of bytes in hex to write to that address.
other part is the data in hex, without spaces between values.
So how I can set filters? There must be change in this script, but what?
I will appreciate any further help. Thanks in advance.
Best regards,
Petar