I'm using the PCM2912A EVM and in the PC works great. However in the Mac (a MacBook Pro) there is a continuous pop coming out of the output channels. Both left and right.
The pop comes out every 1 second or so, as long as the USB codec is selected as the output in the Mac.
I know in the past there was a silicon issue with PCM2912 where a pop was present in the recording channel. That pop in the recording channel was due to excess in the max-packet size and was address in the silicon rev A. (see PDF below)
http://www.ti.com/lit/er/slaz048a/slaz048a.pdf
Now I'm wondering if I came across a new bug in the PCM2912A silicon. Any thoughts?
Thanks,
Igor