This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SYS_RESET and BOOT_RESET

Hi,

Questions concerning interpretation of the description of the EHIF commands SYS_RESET and BOOT_RESET:

In the description of the commands in CC85xx Family User's Guide the timing requirements operates with the 4 parameters ta, tb, tc, td.

1) Under ta the following is stated: "1 us or more. If CC85xx is powered down, add a 2 ms delay before proceeding". Does this 2 ms delay apply after normal initial power-up? Or does it apply only after an explicit power-down command?

2) Under tb is stated "4 us or more" for SYS_RESET, but 4-10 us for BOOT_RESET. Is this a misprint, or could tb be arbitrarily long for SYS_RESET?

3) Under tc is stated "1 us or more", but "Approx. 1 us" for BOOT_RESET. Is this a misprint, or could tc be arbitrarily long for SYS_RESET?

4) What is "Approx. 1 us"? E.g. between 0.5 and 1.5 us?

I have seen a thread in the list mention an errata for the CC85xx. Does such an errata exist? If it does, please point me to where I can get it.

I hope somebody from TI will answer these questions.

Best regards

Ole