Hi All,
Posting my query for the device selection for our own customized board based on OMAPL138 soc, which has integrated AIC3256 code chip for various functionality such as:-
1) Active Noise Reduction (ANR)
2) Passive Noise Reduction (PNR)
3) Echo Cancellation (EC)
4) Echo Suppression (ES)
5) VAD, etc
I can get the details from the data-sheet of AIC3256 supporting EC and ANR, but under the heading Advanced DSP algorithms, how many things are covered.
Like VAD, if supported then its parameters range, etc.
As we are in the phase of selecting device with at-least above mentioned functionalities.
So can you guys help us with some features comparison among devices (like AIC3253, AIC3254, AIC3262, AIC3263, AIC3268 etc) which covers our requirement and which is better and why?
Help will be much appreciated.
Regards
Rishabh Jain