Hi,
I am configuring a TPA3123D2 and I am interested to know more about the power ground and analog ground! Why this separation?? Because after all these two grounds are connected in Power Ground and so they are the same ground!
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am configuring a TPA3123D2 and I am interested to know more about the power ground and analog ground! Why this separation?? Because after all these two grounds are connected in Power Ground and so they are the same ground!
Thank you
Hi Vitor,
They are the same ground with different names. Same name would have avoided this confusion. Connect all the ground pins with a solid ground plane. I would suggest follow the EVM layout for your design.
reg,
Paul Chen
Audio Apps
Hi Paul,
Thank you for your feedback!
I am some confused about this two different grounds! I made some research about this issue and I found some information that explain the diferences about this two grounds. The main reason is about the noise introduzed by different voltages (signal and power), and the solution will be connect the two grounds (in this case in termal pad) via inductor.
Can you give me some feedback about this technique and it can be applicable to this structure? If yes, can you recommend a value for this inductor?
Thank you a lot,
Vitor
No, you must connect the two ground directly.
Regarding noise, I presume that they refer to ground loop. In that case, you just need to avoid routing heavy current flow (output stage to power ground) near any sensitive analog circuitry (input stage, feedback and compensation to analog ground). Merely separating the two ground (ex. output stage to the right of IC and input stage to the left of IC) and only connect them at one point (usually at the thermal pad) is sufficient.
If noise is critical, then consider to use amp with differential input.