Hi all,
I have some questions about DCE specification.
Q1: According to the datasheet of TAS5670MD of P7, DCE (thres) is 2.6V as a typical value.
However, explanation of P33 is mentioned that this value is the minimum output offset voltage.
Which is the right expression in "typical threshold voltage" or the "minimum output offset voltage"?
P33: DC DETECT PROTECTION
The minimum output offset voltages required to trigger the DC detect are show in Table 2. The outputs must
remain at or above the voltage listed in the table for more than 420 msec to trigger the DC detect.
Q2: The dasheet described that "The TAS5760MD has circuitry which will protect the speakers from DC current
which might occur due to an internal amplifier error."
What kind of case are considered as a possibility of an internal error?
When an error occurs, can the device return normally? Is there any possibility of break?
Regards,
Toshi