Hello
I have designed an amplifier with TAS5709. It works very well. Now I am about building a system with several (6) amplifiers, that will be independently controlled over the I2C interface.
My problem: Can I address these six amplifiers DIRECTLY through an I2C bus?
As far as I can see, there is only one address given to each unit (0x36). This address can be changed by software to only one other address (0x38). There are no hardware pins to set the address!
Is there any way to use several circuits on a I2C bus?
I would be thankful if I don't have to build a separate I2C address decoder for this project!
Best regrds, Dan Backlund, Electrobrains