Hi,
I've an inquiry regarding the TPA6141.
Background: The application is BT headphone and also support direct line-in from headphone jack. During active mode (BT enable, power on), audio signal will route to the IC. And in passive mode (user plug in the headphone jack, BT disabled), the audio signal is bypassing the IC as shown in the diagram below:
I've two questions:
1. Is this IC able to support/working in this connection?
2. If yes, what is the absolute maximum rating at OUTR/OUTL before breakdown? (Audio input from passive mode is 1Vrms)