This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Biquad Coefficient calculations using the TI calculator for the TAS5508 GUI

Hi

  I'm trying to calculate the coefficients to use in the TAS5508 GUI, I found the TI Biquad Coefficient Calculator but the the numbers do not seem to produce the same results in the GUI. I assume I'm missing something silly.

I want to produce a low pass filter >100Hz with a bit of a boost at 40Hz. When I plug the numbers in to the 5508 GUI, it shows no filtering and I get a gain increase after 10kHz.. I'd send pics but they will not paste in to this.

 

This is what I get out of the calculator.

Text "* Sample Rate = 48000"
Text "* Filter 1 Low Pass 1st Order Butterworth, 100 Hz Fc 0.0 dB "
Text "* Filter 2 EQ 43 Hz Fc 3.0 dB 10 Hz BW"
Text "* H(z) = (N0 + 2*N1/z + N2/(z2)) / (32768 - 2*D1/z - D2/(z2))"
Text "* Filter Coefficients in format N0, N1, N2, D1, D2"
Text "* Filter 1"
0x00D51314
0x006A898A
0x00000000
0x3F2AECEB
0x00000000
Text "* Filter 2"
0x7FFFFFFF
0x801EC8E7
0x7FC377B8
0x7FEA0C75
0x802ADD7D