Hi,
Could you please give us the measurement data of TAS5624A's frequency response when using TAS5538/TAS5548/TAS5558 as the pwm modulator?
The evaluated conditions which we would like to obtain are shown as below.
Although the frequency range depends on coefficients of LC filter, we would like to confirm whether the high cut-off frequency is over fs/2 of the nyquist frequency.
<Conditions>
PWM Modulator : TAS5538, TAS5548 and TAS5558
Sampling Rate : 96kHz and 192kHz(Native Audio Processing)
Sweep Frequency Range : 20Hz to 100kHz
Best Regards,
Kato