Dear, All
It is a question which is FAUL of TPA3111D1-Q1.
The following things are indicated in the item of "DC Detect" of a datasheet.
When an output is judged to be a short circuit, "/FAULT pin" is driven to low.
When a noise rides on "OUTP/N pin" from the exterior and voltage becomes less than 0V, is an output judged to be a short circuit and drive "/FAULT pin"?
Voltage is about -0.6V and, as for the noise assumed, the cycle of pulse is about 12 uS.
The cycle is 2mS about.
Please let me know the above thing on condition of the following.
- SD on
- SD off
Thanks, Masami M.