This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM9211 ADC phase

Other Parts Discussed in Thread: PCM9211

Hello,

Sorry such a fundamental questions.
My client have a questions about PCM9211, p91 Register # 49h  ADC Function
Control:

(ADPHASE : Default is Normal Input).


* Question 1
Default means that the phase from ADC input to Digital ouput is out of phase(inverting)?
Cline t also saw Fig48 p60 and inverting should be ' normal '.

* Question 2


My understanding is To change the ADC phase by resgister setting , just write ADPHASE=1.
Is it correct?
Any register setting  should be written except 49h?

Please let me know soon ( wtihin 3 days)

Best Regards